Is there a sample somewhere, that shows how to utilize HS USB on the Kinetis devices that support it - specifically, K65/K26?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there a sample somewhere, that shows how to utilize HS USB on the Kinetis devices that support it - specifically, K65/K26?

跳至解决方案
1,376 次查看
alexfeinman
Contributor III

I have a K26 project where the device is used as a USB bridge to connect a set of remote peripherals to the host. Previously it has been using K22, but now that I need to service even more components, I'd like no longer be restricter by USB FS. So two questions I had in mind:

1) Am I right that K26 does not require an external PHY for HS mode and

2) IS there a sample that expose HS USB controller at least to the SDK level (no class implementations, just a vendor device)?

标签 (1)
0 项奖励
回复
1 解答
1,217 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Alex

1. Yes, there is no need an external PHY in your circuit.

2. Sorry, there is no example now. But you can wait KSDK version 1.3.

Best Regards

Paul

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,218 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Alex

1. Yes, there is no need an external PHY in your circuit.

2. Sorry, there is no example now. But you can wait KSDK version 1.3.

Best Regards

Paul

0 项奖励
回复
1,217 次查看
alexfeinman
Contributor III

Thank you. Don't suppose you have an ETA for SDK 1.3?

0 项奖励
回复