Is there a sample somewhere, that shows how to utilize HS USB on the Kinetis devices that support it - specifically, K65/K26?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a sample somewhere, that shows how to utilize HS USB on the Kinetis devices that support it - specifically, K65/K26?

ソリューションへジャンプ
1,394件の閲覧回数
alexfeinman
Contributor III

I have a K26 project where the device is used as a USB bridge to connect a set of remote peripherals to the host. Previously it has been using K22, but now that I need to service even more components, I'd like no longer be restricter by USB FS. So two questions I had in mind:

1) Am I right that K26 does not require an external PHY for HS mode and

2) IS there a sample that expose HS USB controller at least to the SDK level (no class implementations, just a vendor device)?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,235件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Alex

1. Yes, there is no need an external PHY in your circuit.

2. Sorry, there is no example now. But you can wait KSDK version 1.3.

Best Regards

Paul

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,236件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Alex

1. Yes, there is no need an external PHY in your circuit.

2. Sorry, there is no example now. But you can wait KSDK version 1.3.

Best Regards

Paul

0 件の賞賛
返信
1,235件の閲覧回数
alexfeinman
Contributor III

Thank you. Don't suppose you have an ETA for SDK 1.3?

0 件の賞賛
返信