Is there a sample somewhere, that shows how to utilize HS USB on the Kinetis devices that support it - specifically, K65/K26?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a sample somewhere, that shows how to utilize HS USB on the Kinetis devices that support it - specifically, K65/K26?

Jump to solution
2,073 Views
alexfeinman
Contributor III

I have a K26 project where the device is used as a USB bridge to connect a set of remote peripherals to the host. Previously it has been using K22, but now that I need to service even more components, I'd like no longer be restricter by USB FS. So two questions I had in mind:

1) Am I right that K26 does not require an external PHY for HS mode and

2) IS there a sample that expose HS USB controller at least to the SDK level (no class implementations, just a vendor device)?

Labels (1)
0 Kudos
Reply
1 Solution
1,914 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Alex

1. Yes, there is no need an external PHY in your circuit.

2. Sorry, there is no example now. But you can wait KSDK version 1.3.

Best Regards

Paul

View solution in original post

0 Kudos
Reply
2 Replies
1,915 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Alex

1. Yes, there is no need an external PHY in your circuit.

2. Sorry, there is no example now. But you can wait KSDK version 1.3.

Best Regards

Paul

0 Kudos
Reply
1,914 Views
alexfeinman
Contributor III

Thank you. Don't suppose you have an ETA for SDK 1.3?

0 Kudos
Reply