Is there a 'DSPI eDMA Demo' project in KSDK v1.1.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a 'DSPI eDMA Demo' project in KSDK v1.1.0?

Jump to solution
1,929 Views
bradsundstrom
Contributor II

What happened to the DSPI eDMA Demo example project in the KSDK 1.1.0? It was available in KSDK 1.0.0, however, it appears to be missing from KSDK 1.1.0. Was there a known issue with the 1.0.0 implementation that caused it to be removed from the 1.1.0 version?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,667 Views
ivadorazinova
NXP Employee
NXP Employee

Hi dear Brad Sundstrom,

the demo example is not in new version KSDK 1.1.

Because KSDK 1.1. and newer versions integrates DMA feature into the DSPI driver.

Best Regards,

Iva

View solution in original post

0 Kudos
Reply
1 Reply
1,668 Views
ivadorazinova
NXP Employee
NXP Employee

Hi dear Brad Sundstrom,

the demo example is not in new version KSDK 1.1.

Because KSDK 1.1. and newer versions integrates DMA feature into the DSPI driver.

Best Regards,

Iva

0 Kudos
Reply