Is there a 'DSPI eDMA Demo' project in KSDK v1.1.0?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a 'DSPI eDMA Demo' project in KSDK v1.1.0?

ソリューションへジャンプ
2,616件の閲覧回数
bradsundstrom
Contributor II

What happened to the DSPI eDMA Demo example project in the KSDK 1.1.0? It was available in KSDK 1.0.0, however, it appears to be missing from KSDK 1.1.0. Was there a known issue with the 1.0.0 implementation that caused it to be removed from the 1.1.0 version?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,354件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi dear Brad Sundstrom,

the demo example is not in new version KSDK 1.1.

Because KSDK 1.1. and newer versions integrates DMA feature into the DSPI driver.

Best Regards,

Iva

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,355件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi dear Brad Sundstrom,

the demo example is not in new version KSDK 1.1.

Because KSDK 1.1. and newer versions integrates DMA feature into the DSPI driver.

Best Regards,

Iva

0 件の賞賛
返信