Is there a 'DSPI eDMA Demo' project in KSDK v1.1.0?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there a 'DSPI eDMA Demo' project in KSDK v1.1.0?

跳至解决方案
2,593 次查看
bradsundstrom
Contributor II

What happened to the DSPI eDMA Demo example project in the KSDK 1.1.0? It was available in KSDK 1.0.0, however, it appears to be missing from KSDK 1.1.0. Was there a known issue with the 1.0.0 implementation that caused it to be removed from the 1.1.0 version?

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
2,331 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi dear Brad Sundstrom,

the demo example is not in new version KSDK 1.1.

Because KSDK 1.1. and newer versions integrates DMA feature into the DSPI driver.

Best Regards,

Iva

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,332 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi dear Brad Sundstrom,

the demo example is not in new version KSDK 1.1.

Because KSDK 1.1. and newer versions integrates DMA feature into the DSPI driver.

Best Regards,

Iva

0 项奖励
回复