Installing KSDK on Ubuntu 64-bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installing KSDK on Ubuntu 64-bit

1,400 Views
midnight
Contributor I

Is there a procedure for getting the KSDK installed on Ubuntu 17.04 and all the other files needed for developing for the TWR-K65F180M?

Thanks,

K-

0 Kudos
Reply
1 Reply

1,290 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Kyle Unice

I hear from a colleague that you problem has been resolved in a case. The problem seams to be related with your tower serial connections and power supply, can you confirm that you problem has been resolved?

If the problem still exists could you explain more your issue? as you can see in the image below, you can download KSDK for linux:

pastedImage_1.png

Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply