Installing KSDK on Ubuntu 64-bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing KSDK on Ubuntu 64-bit

1,360件の閲覧回数
midnight
Contributor I

Is there a procedure for getting the KSDK installed on Ubuntu 17.04 and all the other files needed for developing for the TWR-K65F180M?

Thanks,

K-

0 件の賞賛
返信
1 返信

1,250件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Kyle Unice

I hear from a colleague that you problem has been resolved in a case. The problem seams to be related with your tower serial connections and power supply, can you confirm that you problem has been resolved?

If the problem still exists could you explain more your issue? as you can see in the image below, you can download KSDK for linux:

pastedImage_1.png

Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信