I have no processors or boards available when creating a new project in KDS V2.0. I tried reinstalling KDS, still the same. I am running Win 10 64 bit on a core i7. I want to use my FRDM KL25Z board to begin with

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I have no processors or boards available when creating a new project in KDS V2.0. I tried reinstalling KDS, still the same. I am running Win 10 64 bit on a core i7. I want to use my FRDM KL25Z board to begin with

1,081 次查看
petersommer
Contributor I

The window says "contains processors" or "contains board support" but there is nothing there. I can'@t move on from here.

标签 (1)
0 项奖励
回复
2 回复数

900 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Peter!

1) Please, go to https://nxp.flexnetoperations.com/control/frse/product?entitlementId=123521727&lineNum=1&authContact...  and download the newest KDS v.3.2.0, please see also New Kinetis Design Studio v3.2.0 available

2) do you want to create new KSDK project? If yes, you should have downloaded package for your KL25Z from http://kex.freescale.com/ with the procedure described here How to: install KSDK 2.0 and create new project via wizard or project generator tool, please see New Kinetis SDK Project Generator v2 is available!

wizard.png

Please let me know in case of any issue,

Best Regards,

Iva

0 项奖励
回复

900 次查看
petersommer
Contributor I

It is actually KDS V3.2. sorry.

0 项奖励
回复