I get misteke during compilation.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I get misteke during compilation.

ソリューションへジャンプ
3,618件の閲覧回数
profprogrammer
Contributor III

Hi.

 

I used  KSDK and I receive a mistake during compilation.

arm-none-eabi-g++: error: ./SDK/plaform/drivers/src/pit/fsl_pit_common.o: No such file or directory

 

But this file is in this folder.

Why the linker can't find this file?

 

Here so the report of the compiler looks.

09:32:27 **** Incremental Build of configuration Debug for project nmk5 **** make all  'Building target: nmk5.elf' 'Invoking: Cross ARM C++ Linker' arm-none-eabi-g++ -mcpu=cortex-m4 -mthumb -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g -T "D:/vn/proj/KSDK_ip/nmk5/Project_Settings/Linker_Files/ProcessorExpert.ld" -Xlinker --gc-sections -L"D:/vn/proj/KSDK_ip/nmk5/Project_Settings/Linker_Files" -Wl,-Map,"nmk5.map" -specs=nosys.specs  -lgcc -lc -lsupc++ -lm -nostartfiles -Xlinker -z -Xlinker muldefs -Xlinker -static -o "nmk5.elf"  ./lwip/src/netif/ppp/auth.o ./lwip/src/netif/ppp/chap.o ./lwip/src/netif/ppp/chpms.o ./lwip/src/netif/ppp/fsm.o ./lwip/src/netif/ppp/ipcp.o ./lwip/src/netif/ppp/lcp.o ./lwip/src/netif/ppp/magic.o ./lwip/src/netif/ppp/md5.o ./lwip/src/netif/ppp/pap.o ./lwip/src/netif/ppp/ppp.o ./lwip/src/netif/ppp/ppp_oe.o ./lwip/src/netif/ppp/randm.o ./lwip/src/netif/ppp/vj.o  ./lwip/src/netif/etharp.o ./lwip/src/netif/slipif.o  ./lwip/src/core/snmp/asn1_dec.o ./lwip/src/core/snmp/asn1_enc.o ./lwip/src/core/snmp/mib2.o ./lwip/src/core/snmp/mib_structs.o ./lwip/src/core/snmp/msg_in.o ./lwip/src/core/snmp/msg_out.o  ./lwip/src/core/ipv4/autoip.o ./lwip/src/core/ipv4/icmp.o ./lwip/src/core/ipv4/igmp.o ./lwip/src/core/ipv4/inet.o ./lwip/src/core/ipv4/inet_chksum.o ./lwip/src/core/ipv4/ip.o ./lwip/src/core/ipv4/ip_addr.o ./lwip/src/core/ipv4/ip_frag.o  ./lwip/src/core/def.o ./lwip/src/core/dhcp.o ./lwip/src/core/dns.o ./lwip/src/core/init.o ./lwip/src/core/lwip_timers.o ./lwip/src/core/mem.o ./lwip/src/core/memp.o ./lwip/src/core/netif.o ./lwip/src/core/pbuf.o ./lwip/src/core/raw.o ./lwip/src/core/stats.o ./lwip/src/core/sys.o ./lwip/src/core/tcp.o ./lwip/src/core/tcp_in.o ./lwip/src/core/tcp_out.o ./lwip/src/core/udp.o  ./lwip/src/api/api_lib.o ./lwip/src/api/api_msg.o ./lwip/src/api/err.o ./lwip/src/api/netbuf.o ./lwip/src/api/netdb.o ./lwip/src/api/netifapi.o ./lwip/src/api/sockets.o ./lwip/src/api/tcpip.o  ./lwip/port/ethernetif.o ./lwip/port/lwip_fsl_irq.o ./lwip/port/sys_arch.o  ./Static_Code/System/PE_low_level_init.o ./Static_Code/System/Peripherals_Init.o  ./Static_Code/Peripherals/ENET_Init.o  ./Sources/Events.o ./Sources/fsl_phy_driver.o ./Sources/main.o ./Sources/os_tasks.o ./Sources/rtos_main_task.o  ./SDK/rtos/mqx/mqx_stdlib/source/strings/strings.o  ./SDK/rtos/mqx/mqx_stdlib/source/stdio/buf_prv.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/err.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/fclose.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/fflush.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/fopen.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/fp_prv.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/fread.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/fwrite.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/get.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/pos.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/print.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/print_prv.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/put.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/scan.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/scan_prv.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/stdio.o  ./SDK/rtos/mqx/mqx/source/string/str_utos.o ./SDK/rtos/mqx/mqx/source/string/strnlen.o  ./SDK/rtos/mqx/mqx/source/psp/cortex_m/core/M4/boot.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/core/M4/dispatch.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/core/M4/support.o  ./SDK/rtos/mqx/mqx/source/psp/cortex_m/compiler/gcc_arm/comp.o  ./SDK/rtos/mqx/mqx/source/psp/cortex_m/cortex.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/int_gkis.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/int_kisr.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/int_pvta.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/int_unx.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/int_vtab.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/int_xcpt.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/ipsum.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/mem_copy.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/mem_zero.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/nvic.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_dati.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_gelms.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_hoti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_iinit.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_mat1.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_mat2.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_mat3.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_miti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_msti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_mstiq.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_nsti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_psti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_seti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_supp.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tiad.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tida.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tihr.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_timn.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tims.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tinm.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tins.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tiol.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tipr.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tips.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tise.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tisu.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tius.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tkti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_usti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/sc_irdyq.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/stack_bu.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/stack_de.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/stack_st.o  ./SDK/rtos/mqx/mqx/source/nio/src/errno.o ./SDK/rtos/mqx/mqx/source/nio/src/nio.o ./SDK/rtos/mqx/mqx/source/nio/src/nio_posix.o ./SDK/rtos/mqx/mqx/source/nio/src/nio_std_adpt.o  ./SDK/rtos/mqx/mqx/source/nio/fs/fs_supp.o  ./SDK/rtos/mqx/mqx/source/nio/drivers/nio_tty/src/nio_tty.o  ./SDK/rtos/mqx/mqx/source/nio/drivers/nio_serial/src/nio_serial.o  ./SDK/rtos/mqx/mqx/source/nio/drivers/nio_dummy/src/nio_dummy.o  ./SDK/rtos/mqx/mqx/source/kernel/event.o ./SDK/rtos/mqx/mqx/source/kernel/idletask.o ./SDK/rtos/mqx/mqx/source/kernel/inittask.o ./SDK/rtos/mqx/mqx/source/kernel/int.o ./SDK/rtos/mqx/mqx/source/kernel/klog.o ./SDK/rtos/mqx/mqx/source/kernel/log.o ./SDK/rtos/mqx/mqx/source/kernel/lwevent.o ./SDK/rtos/mqx/mqx/source/kernel/lwlog.o ./SDK/rtos/mqx/mqx/source/kernel/lwmem.o ./SDK/rtos/mqx/mqx/source/kernel/lwmsgq.o ./SDK/rtos/mqx/mqx/source/kernel/lwsem.o ./SDK/rtos/mqx/mqx/source/kernel/lwtimer.o ./SDK/rtos/mqx/mqx/source/kernel/mem.o ./SDK/rtos/mqx/mqx/source/kernel/mqx.o ./SDK/rtos/mqx/mqx/source/kernel/msg.o ./SDK/rtos/mqx/mqx/source/kernel/msgpool.o ./SDK/rtos/mqx/mqx/source/kernel/msgq.o ./SDK/rtos/mqx/mqx/source/kernel/mutex.o ./SDK/rtos/mqx/mqx/source/kernel/name.o ./SDK/rtos/mqx/mqx/source/kernel/partition.o ./SDK/rtos/mqx/mqx/source/kernel/queue.o ./SDK/rtos/mqx/mqx/source/kernel/sched.o ./SDK/rtos/mqx/mqx/source/kernel/sem.o ./SDK/rtos/mqx/mqx/source/kernel/task.o ./SDK/rtos/mqx/mqx/source/kernel/taskq.o ./SDK/rtos/mqx/mqx/source/kernel/time.o ./SDK/rtos/mqx/mqx/source/kernel/timer.o ./SDK/rtos/mqx/mqx/source/kernel/tlsf.o ./SDK/rtos/mqx/mqx/source/kernel/tlsf_adaptation.o ./SDK/rtos/mqx/mqx/source/kernel/watchdog.o  ./SDK/rtos/mqx/mqx/source/bsp/init_bsp.o  ./SDK/platform/system/src/interrupt/fsl_interrupt_manager.o  ./SDK/platform/system/src/hwtimer/fsl_hwtimer.o ./SDK/platform/system/src/hwtimer/fsl_hwtimer_pit.o ./SDK/platform/system/src/hwtimer/fsl_hwtimer_systick.o  ./SDK/platform/system/src/clock/MK60D10/fsl_clock_MK60D10.o  ./SDK/platform/system/src/clock/fsl_clock_manager.o ./SDK/platform/system/src/clock/fsl_clock_manager_common.o  ./SDK/platform/osa/src/fsl_os_abstraction_mqx.o  ./SDK/platform/hal/src/uart/fsl_uart_hal.o  ./SDK/platform/hal/src/sim/MK60D10/fsl_sim_hal_MK60D10.o  ./SDK/platform/hal/src/rtc/fsl_rtc_hal.o  ./SDK/platform/hal/src/port/fsl_port_hal.o  ./SDK/platform/hal/src/pit/fsl_pit_hal.o  ./SDK/platform/hal/src/osc/fsl_osc_hal.o  ./SDK/platform/hal/src/mpu/fsl_mpu_hal.o  ./SDK/platform/hal/src/mcg/fsl_mcg_hal.o ./SDK/platform/hal/src/mcg/fsl_mcg_hal_modes.o  ./SDK/platform/hal/src/enet/fsl_enet_hal.o  ./SDK/platform/drivers/src/uart/fsl_uart_common.o ./SDK/platform/drivers/src/uart/fsl_uart_driver.o  ./SDK/platform/drivers/src/rtc/fsl_rtc_common.o  ./SDK/platform/drivers/src/pit/fsl_pit_common.o  ./SDK/platform/drivers/src/mpu/fsl_mpu_common.o ./SDK/platform/drivers/src/mpu/fsl_mpu_driver.o  ./SDK/platform/drivers/src/enet/fsl_enet_common.o ./SDK/platform/drivers/src/enet/fsl_enet_driver.o  ./SDK/platform/devices/MK60D10/startup/gcc/startup_MK60D10.o  ./SDK/platform/devices/MK60D10/startup/system_MK60D10.o  ./SDK/platform/devices/startup.o  ./Generated_Code/Cpu.o ./Generated_Code/MainTask.o ./Generated_Code/Task1.o ./Generated_Code/Task2.o ./Generated_Code/clockMan1.o ./Generated_Code/eNet1.o ./Generated_Code/fsl_hwtimer1.o ./Generated_Code/fsl_mpu1.o ./Generated_Code/hardware_init.o ./Generated_Code/hwTim1.o ./Generated_Code/mqx_ksdk.o ./Generated_Code/osa1.o ./Generated_Code/pin_mux.o ./Generated_Code/uart1.o    arm-none-eabi-g++: error: ./SDK/plaform/drivers/src/pit/fsl_pit_common.o: No such file or directory make: *** [nmk5.elf] Error 1

Original Attachment has been moved to: nmk7.zip

ラベル(1)
1 解決策
3,219件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Prof Programmer:

Your console output shows a problem (plaform instead of platform):

pastedImage_0.png

And there is a large list of parameters in the linker call, so you are definitely running into the 8192 characters command line limit in Windows. Please see the next tutorial on how to solve it.

Solving the 8192 Character Command Line Limit on Windows | MCU on Eclipse

Regards!

Jorge Gonzalez

元の投稿で解決策を見る

6 返答(返信)
3,220件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Prof Programmer:

Your console output shows a problem (plaform instead of platform):

pastedImage_0.png

And there is a large list of parameters in the linker call, so you are definitely running into the 8192 characters command line limit in Windows. Please see the next tutorial on how to solve it.

Solving the 8192 Character Command Line Limit on Windows | MCU on Eclipse

Regards!

Jorge Gonzalez

3,219件の閲覧回数
jamiepacker
Contributor II

It may be worth noting that the SOMNIUM DRT IDE for Kinetis includes a fix for the 8192 character command line program. Just one of the little things we do to make life easier for developers. :smileywink:

0 件の賞賛
返信
3,219件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Prof Programmer,

please is it possible to send us your screenshot of Properties for fsl_pit_common.c ? Or upload your project here for us?

Thank you,

Best Regards,

Iva

0 件の賞賛
返信
3,219件の閲覧回数
profprogrammer
Contributor III

Here my screenshot of fsl_pit_common.c properties.

1.jpg

My project.

https://community.freescale.com/servlet/JiveServlet/download/579756-364812/nmk7.zip

0 件の賞賛
返信
3,219件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Please click on 'Project' menu-> Clean to remove the object file and rebuild again. Does it work?

If not, please double click on the file ‘fsl_pit_common.c’, can this file be opened in KDS editor window?  And right click on the file to select ‘Properties’, is its path and location displayed in the pop-up window correct? 

fsl_pit.png

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,219件の閲覧回数
profprogrammer
Contributor III

I tried these actions didn't help to isprativit a mistake.

0 件の賞賛
返信