Hello!
I would like to know how to install KSDK 1.2.0 on Linux machines. I've downloaded it from KSDK website, and unziped it (using gunzip app). Instead of a directory full of code, I got a giant XML-like file.
Any help?
Cheers,
Ronaldo
解決済! 解決策の投稿を見る。
 
					
				
		
 BlackNight
		
			BlackNight
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		For the Kinetis SDK on Linux: There is a 2 step process in extracting the files before you can read the readme.
The first extraction is the .gz -> tar. The gz is a compacted file 623MB, and the tar file is not compressed and is 2.6G. One then needs to extract the files from the tar. Then you can can read the docs.
I hope this helps.
Erich
FYI: I have submitted a change request to have this improved for the future.
 
					
				
		
Just to add extra info this.
After extracting the "Kinetis SDK 1.2.0 Mainline - Linux.gz" (623MB) file you will get the "Kinetis SDK 1.2.0 Mainline - Linux" (2.6GB) file.
Then extract it with the command: "tar -xvf Kinetis\ SDK\ 1.2.0\ Mainline\ -\ Linux"
 
					
				
		
Now I'm facing with a problem.
When I Try to install "KSDK_1.2.0_Eclipse_Update.zip" On Kinetis Design Studio I'm getting this message:
"An error occurred while collecting items to be installed
session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No repository found containing: binary,com.somniumtech.kds.executable.gtk.linux.x86_64,3.0.0"
I'm on Ubuntu 14.04 64bits.
I had the same problem. Run Kinetis Design Studio as root:
sudo /opt/Freescale/KDS_3.0.0/eclipse/kinetis-design-studio
then install update.
 
					
				
		
Thanks,
It worked.
 
					
				
		
Thanks Erich and David! Your answers solved the question.
Regards,
Ronaldo
 
					
				
		
 BlackNight
		
			BlackNight
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		For the Kinetis SDK on Linux: There is a 2 step process in extracting the files before you can read the readme.
The first extraction is the .gz -> tar. The gz is a compacted file 623MB, and the tar file is not compressed and is 2.6G. One then needs to extract the files from the tar. Then you can can read the docs.
I hope this helps.
Erich
FYI: I have submitted a change request to have this improved for the future.
 
					
				
		
I'm hoping the change request includes changing the suffix of the download from .gz to .tgz or .tar.gz?
 
					
				
		
 DavidS
		
			DavidS
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Ronaldo,
Please look at the last two posts at very bottom on the web page:
New Kinetis Design Studio V3.0.0 available
File needs to be renamed with .deb extension then "sudo dpkg -i *.deb" to install.
Regards,
David