How low power drivers differ from standard drivers?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How low power drivers differ from standard drivers?

ソリューションへジャンプ
1,771件の閲覧回数
laszlomonda
Contributor V

Hi guys,

 

I've noticed that there are low power versions of standard drivers, like LPI2C vs I2C, LPUART vs UART, and interestingly LPTMR, without a TMR counterpart. How those drivers differ from each other? Please bear in mind that I'm new to the Kinetis platform, so you're welcome to explain the basics if needed.

 

Thanks!

- Laci

ラベル(1)
タグ(3)
1 解決策
1,262件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Laci,

They are not the low power version of standard drivers, actually there are modules with low power enhancement , like LPUART module and UART module, but they are different modules, so they have different drivers in KSDK 2.x.

Hope that makes sense,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,263件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Laci,

They are not the low power version of standard drivers, actually there are modules with low power enhancement , like LPUART module and UART module, but they are different modules, so they have different drivers in KSDK 2.x.

Hope that makes sense,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------