How correct use of Backdoor Key in FRDM-KL82Z board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How correct use of Backdoor Key in FRDM-KL82Z board

1,405件の閲覧回数
rysardsuboc
Contributor II

I use official board and SDK libraries. I write my project in MDK.

I set the MCU in secure status and enabled backdoor key access.

 

When I use FLASH_SecurityBypass() function from library, function returned me FLASH Access Error status.

I entered the same backdoor key which is in FCCOB registers. For key entering I use terminal window.

 

The problem comes from FLASH_SecurityBypass() function where call flash_command_sequence() function. 

flash_command_sequence() function returned FLASH Access Error status.

ラベル(1)
0 件の賞賛
返信
1 返信

1,171件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Rysard,

You can try to use the attached pflash.c and startup_MKL82Z7.s test on your FRDM-KL82Z board.

Using pflash exmaple in SDK_2.0_FRDM-KL82Z.

pflash SDK_2.0_FRDM-KL82Z.png

In startup_MKL82Z7.s file I have the following key entered:

/* Flash Configuration */

    .section .FlashConfig, "a"

    .long 0x01020304 /* //DES was 0xFFFFFFFF */

    .long 0x05060708 /* //DES was 0xFFFFFFFF */

    .long 0xFFFFFFFF

    .long 0xFFFFFFBC /* //DES enable BackDoorKey and lock flash=0xFFFFFFBC was 0xFFFFFFFE */

 

Using pflash.c I added test code:

uint8_t MyBackDoorKey[]={0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08};//DES test works

The terminal output is:

terminal output.png

 

The Count down gave me time to plug in the FRDM-KL82Z, let the VCOM enumerate, and then allow the terminal window to be open.

I loaded the example and modified it.  The two source files attached in ZIP file for reference.

 

Folder locations:

C:\SDK_2.0_FRDM-KL82Z\boards\frdmkl82z\driver_examples\flash\pflash.c

C:\SDK_2.0_FRDM-KL82Z\devices\MKL82Z7\iar\startup_MKL82Z7.s

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信