FreeRTOS for MKL16z128VFM4(FRDM KL-26Z)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS for MKL16z128VFM4(FRDM KL-26Z)

10,752 Views
vipinkumar27
Contributor II

Hi,

 

I am using FRDM KL-26z board for MKL16z128VFM4 processor.I am using KSDK v 1.3.0 mainline. I want to use FreeRTOS but I couldn't find the FreeRTOS example or even ,when I opened  Processor expert ,in OSs folder,I couldn't find FreeRTOS .c files.Am I using the correct KSDK ? I am not able to find the way out to FreeRTOS usage in KL26Z.

Labels (1)
0 Kudos
Reply
25 Replies

8,743 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Vipin,

You  can download and install the KSDK2.0, after install , you can find the FreeRTOS demo

as these:

pastedImage_0.png

About the detail method to download and install please refer to :

How to: install KSDK 2.0

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

8,743 Views
vipinkumar27
Contributor II

Thanks a lot.:smileyhappy:

0 Kudos
Reply

8,743 Views
vipinkumar27
Contributor II

Does it support MKL16z128VfM4?

0 Kudos
Reply

8,743 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Yes,

pastedImage_0.png


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

8,743 Views
vipinkumar27
Contributor II

Hi,whenever I am pressing Select Configuration after selecting Board-FRDMKL26Z,its not moving forward and returns back to the same page without any error.I tried it randomly by selecting other boards too but  same is happening .

Is there any other way to get ksdk2.0 for FRDM -KL26Z ?

0 Kudos
Reply

8,743 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Vipin,

Please take a screenshot about your process and the error , thank !

BR

Alice

0 Kudos
Reply

8,743 Views
vipinkumar27
Contributor II

Screen Shot 2016-02-22 at 2.33.54 PM.pngScreen Shot 2016-02-22 at 2.36.52 PM.pngScreen Shot 2016-02-22 at 2.37.29 PM.pngScreen Shot 2016-02-22 at 2.38.08 PM.pngScreen Shot 2016-02-22 at 2.38.29 PM.png

0 Kudos
Reply

8,743 Views
vipinkumar27
Contributor II

1st page-Download clicked.

2nd page-Kinetis SDK Builder Download clicked.

3rd page-Build an SDK clicked

4th page-Select Config after selecting FRDM KL26Z

5th page-the same page everytime not moving forward

0 Kudos
Reply

8,743 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Vipin,

please what browser do you use?

BR,

Iva

0 Kudos
Reply

8,743 Views
vipinkumar27
Contributor II

Google chrome but I tried with Internet Explorer and the same thing happened

0 Kudos
Reply

8,743 Views
ivadorazinova
NXP Employee
NXP Employee

Thank your feedback, I will report it.

Please, try it in Firefox, it works without problems.

Please, let me know if it works you.

Best Regards,

Iva

0 Kudos
Reply

8,743 Views
vipinkumar27
Contributor II

It is not working in Mozilla too.

0 Kudos
Reply

8,743 Views
ivadorazinova
NXP Employee
NXP Employee

Please, what do you use for the Firefox version?

You can use for this What browser am I using? Is my browser up to date? Web browser detection, Javascript, Cookies, Flash...

Best Regards,

Iva

0 Kudos
Reply

8,743 Views
vipinkumar27
Contributor II

1 week back,I had downloaded some Ksdk version by building the SDK and this thing was working even in google chrome.

0 Kudos
Reply

8,743 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Vipin,

thank you for the information.

The bug is reported Jira ticket KEX-797

Best Regards,

Iva

0 Kudos
Reply

8,743 Views
vipinkumar27
Contributor II

Can you please share the link for the repository of this file?

Email-id:[email protected]

0 Kudos
Reply

8,743 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Vipin,

we have been working on the issue.

But it is strange that you face the issue also in Firefox 44. I have installed Firefox 44 and it works for me on my side.

Yes, I have share it with you, but FRDM-KL26Z (MKL16Z128xxx4) is supported by KSDK 1.3 not by KSDK 2.0.

Best Regards,

Iva

0 Kudos
Reply

8,743 Views
vipinkumar27
Contributor II

I randomly tried downloading for other boards too but the KSDK2.0 wasn't getting download for anyone of them

0 Kudos
Reply

8,743 Views
vipinkumar27
Contributor II

I want to use FreeRTOS for my coding but couldn't find enough examples in KSDK1.3 and as per the discussion ,I thought KSDK2.0 is supported by KL-26Z.

0 Kudos
Reply

8,743 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Vipin,

there are a lot of examples, but not all of them are for your board.

Please, take a look at demo I2C RTOS located under C:\Freescale\KSDK_1.3.0\examples\frdmkl26z\demo_apps\i2c_rtos\i2c_rtos_freertos

I hope this helps.

Iva

0 Kudos
Reply