Does anybody have experience with the Zephyr Micro/Nano RTOS?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does anybody have experience with the Zephyr Micro/Nano RTOS?

跳至解决方案
1,731 次查看
myke_predko
Senior Contributor III

Gentlebeings,

 

I just saw this announcement (http://linuxgizmos.com/zephyr-a-tiny-open-source-iot-rtos/) on Slashdot discussing the Zephyr RTOS (https://www.zephyrproject.org/content/zephyr-kernel-v100-release-notes).  What caught my eye is that a) it's been implemented for the FRDM-K64F and b) that it can be as small as 10k. 

 

I'm experimenting with freeRTOS and for my product, I want to use it along with USB CDC or HID and the FatFs on a 128k Flash sized K22F and things are looking very tight for implementing logic with it. 

 

Thanx,

 

myke

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,226 次查看
Jmart
NXP Employee
NXP Employee

Myke,

As you can imagine, Zephyr is still in its infancy. The 1.0 push that is now accessible does have some K64 support, but it's far from a full platform at this time. I'd continue down the FrerRTOS path that you're on for now and keep an eye on Zephyr as it matures.

Jason

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,227 次查看
Jmart
NXP Employee
NXP Employee

Myke,

As you can imagine, Zephyr is still in its infancy. The 1.0 push that is now accessible does have some K64 support, but it's far from a full platform at this time. I'd continue down the FrerRTOS path that you're on for now and keep an eye on Zephyr as it matures.

Jason

0 项奖励
回复
1,226 次查看
myke_predko
Senior Contributor III

Okay - Thanx!

0 项奖励
回复