Does anybody have experience with the Zephyr Micro/Nano RTOS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does anybody have experience with the Zephyr Micro/Nano RTOS?

ソリューションへジャンプ
2,204件の閲覧回数
myke_predko
Senior Contributor III

Gentlebeings,

 

I just saw this announcement (http://linuxgizmos.com/zephyr-a-tiny-open-source-iot-rtos/) on Slashdot discussing the Zephyr RTOS (https://www.zephyrproject.org/content/zephyr-kernel-v100-release-notes).  What caught my eye is that a) it's been implemented for the FRDM-K64F and b) that it can be as small as 10k. 

 

I'm experimenting with freeRTOS and for my product, I want to use it along with USB CDC or HID and the FatFs on a 128k Flash sized K22F and things are looking very tight for implementing logic with it. 

 

Thanx,

 

myke

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,699件の閲覧回数
Jmart
NXP Employee
NXP Employee

Myke,

As you can imagine, Zephyr is still in its infancy. The 1.0 push that is now accessible does have some K64 support, but it's far from a full platform at this time. I'd continue down the FrerRTOS path that you're on for now and keep an eye on Zephyr as it matures.

Jason

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,700件の閲覧回数
Jmart
NXP Employee
NXP Employee

Myke,

As you can imagine, Zephyr is still in its infancy. The 1.0 push that is now accessible does have some K64 support, but it's far from a full platform at this time. I'd continue down the FrerRTOS path that you're on for now and keep an eye on Zephyr as it matures.

Jason

0 件の賞賛
返信
1,699件の閲覧回数
myke_predko
Senior Contributor III

Okay - Thanx!

0 件の賞賛
返信