Can't Find Kinetis Protocol Decoder Software for USB-KW41Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't Find Kinetis Protocol Decoder Software for USB-KW41Z

5,029 次查看
jgw_sw_eng
Contributor II

Hi all,

I am trying to follow the instructions here to setup wireshark to run with with the USB-KW41Z I just ordered. https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/Use-the-USB-KW41-Wireshark-for-Thread-S...

About half way through the article, it tells me to download the Kinetic Protocol Analyzer here: https://www.nxp.com/webapp/Download?colCode=KINETIS-PRTCL-ANALYZER-ADAPTER&appType=license&l...

However, that page just says: "We are unable to complete your software download request at this time due to a system outage. Please try your download at a later time. We apologize for the inconvenience." I have checked back multiple times over the last few days since my first try, but I still see this error. Is there any other way I can download this software?

0 项奖励
回复
4 回复数

4,881 次查看
mikesores
Contributor I

Many software development teams also provide on-going support after the project is completed. With on-going support, you are less likely to have problems with your system or integration with your business process. Support can be as simple as an email to answer questions or a call if there are issues. Some development teams offer support via a dedicated toll free number, 24 hours a day, seven days a week. Finally, there is cost efficiency. When you hire a dedicated software development team, you will be paying less than you would if you hired on-site staff and your system were integrated with your business. When software development team https://mlsdev.com/services/dedicated-development-team  are hired full-time, you may pay as much as 30% more for labor. Hiring a part-time employee will save you even more money.

0 项奖励
回复

5,020 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Please check the attachment.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

5,010 次查看
jgw_sw_eng
Contributor II

Hi TIC,

Thank you for your help. I have installed that linked file that includes the KPAA installer. However, one of the first steps is to install a TAP-Windows adapter - see the attached screenshot from running the installer. When I click on that "Download and manually install TAP-Windows Adapter", it takes me to a website that is shut down. I tried typing in the URL that is displayed in the message just to confirm, and it appears to be the same link that is shut down.

Are you able to also supply the TAP adapter that is needed. I am on a Windows 10 machine.

Thanks

Jake

NXP TAP Error.pngNXP TAP Error.png

0 项奖励
回复

5,005 次查看
jgw_sw_eng
Contributor II

Apologies, there was a network issue on my side causing the download issue. I was able to install the TAP adapter and install KPAA.

0 项奖励
回复