Are there any USB 5.0 HOST MSC CDC Examples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are there any USB 5.0 HOST MSC CDC Examples

1,086件の閲覧回数
neilhancock
Contributor IV

Hi Support

I'd like to put in a plug for a  USB 5.0 HOST examples in the next SDK release - be really nice to be able to try out USB Host MSC CDC ?

My target is for USB Stick storage and using USB to control a device (modem, IoT weightless device, or other IoT wireless etc)

My experience is the M2M wireless access needs to be encapsulated, and the way to make it plug-n-play is through USB for end user customers.

I've just had some customers shafted when an ATT 2G signal disappearing. Kaput gone. M2M device that had worked for a year useless.

The  M2M remote monitoring device uses a 2G GPRSS modem  with an ATT SIM. There is another local carrier T-Mobile signal, but the embedded modem is so integrated in the electronics that the whole device has to be replaced at great cost. Replacing a SIM is not the answer as sometimes need other wireless devices than GSM 2G 3G 4G....

 

Any other users got applications they can see with USB 5.0 Host ...?

ラベル(1)
0 件の賞賛
返信
1 返信

860件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

I am part of the Support team and I am not sure about the plans for the USB stack 5.0. The information I can provide you is that the new USB stack 5.0 will implement the use of the KSDK drivers with several examples for Host and Device, but I am not up to the information about which composite examples will be available.

The USB stack v5 will provide a document that explains how to create a new composite project and how to port the existing project to a different device. Note that the KSDK + USB stack will only support devices supported by the KSDK drivers.

I hope this information can help you.

Regards,

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. It would be nice!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信