Problem in Torque Control with Hall StartUp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in Torque Control with Hall StartUp

ソリューションへジャンプ
5,755件の閲覧回数
joãopaulo
Contributor III

I'm developing an E-Bike based on KV31F and KMS and I intend to use Torque control with Hall StartUp, but looks like that when the control changes from hall to torque control the three fases of the motor are shorted, because the bicycle wheel stops abruptly, however the system don't show any fault. What could be the cause of this behavior?

Thanks.

 


ラベル(1)
1 解決策
5,226件の閲覧回数
PedroCastro
Contributor III

the problem was solved using the file attached by AdamReynolds‌ in this post:

https://community.nxp.com/thread/471190 

元の投稿で解決策を見る

6 返答(返信)
5,226件の閲覧回数
linestream-adam
Senior Contributor I

Interesting.  There was a bug in the latest KMS with respect to running torque control after hall startup.  The updated file has been posted in this post (see the bottom of the thread): https://community.nxp.com/thread/469770 

I would be curious to hear if you have the same issue after trying with the updated file.

0 件の賞賛
返信
5,226件の閲覧回数
joãopaulo
Contributor III

I work with the guy of the other post.

The problem now isn't reach the rated speed, the problem is that if I set more that 3A for the current mode the motor stops like the three fases were shorted, and seems that higher the current the sooner the motor stops.

If you could support me with some urgency I'd be greatful.

Thanks.

0 件の賞賛
返信
5,226件の閲覧回数
linestream-adam
Senior Contributor I

Gotcha.  I started looking into why the phases shorted, and nothing is jumping out at me as to why that would be happening.  Is the power supply dipping such that the MCU is browning out?  KMS will tell you if the MCU resets.  If you don't have KMS connected, make sure that commTimeOutEnabled in main.c is set to false.

5,226件の閲覧回数
PedroCastro
Contributor III

Hi Adam,

I am working in the same project as João. The MCU does not reset and I don't use the commTimeOutEnabled anymore. It looks to me that when a higher current is set a higher speed is reached faster. When the bikes wheels spins withoud a load, the motor stall even faster. One possible solution would be to enter in COAST mode when in higher speeds but I am not sure if it is possible to go from BRAKE_COAST to RUN_CURRENT withou going through IDLE. If is is in IDLE, the system must be below FOCLowSpeed, correct? However it is not case. Do you have any ideas?

0 件の賞賛
返信
5,227件の閲覧回数
PedroCastro
Contributor III

the problem was solved using the file attached by AdamReynolds‌ in this post:

https://community.nxp.com/thread/471190 

5,226件の閲覧回数
joãopaulo
Contributor III

Thanks very much for the great support Adam Reynolds!

0 件の賞賛
返信