hi
purchased the TWR-K60D100M development and download the com.freescale.mcu10_2.Kinetis_100MHz_K10_K20_K30_K40_K50_K60.win.v1_0_2 from the freescale website and unzip the file and trying to run the content.jar executable file .and getting an error "invalid or corrupted jar file " having Jdk 6 and jre7 version java . Please let me know the solution to problem
thanks
vallinath
解決済! 解決策の投稿を見る。
The "toolkit" you make reference to is a CodeWarrior 10.2 update, it is not an executable file, you need to install it from the CodeWarrior menu in the following manner:
1 Open CodeWarrior 10.2
2 On the upper tool menu click on help > install software
3 Click on the add button to the right of the work with address bar
4 A new window will pop up, click on the archive button and navigate to the root folder where you saved the update file and click ok
thanks works fine
Vallinath, were this suggestions useful?
We'd like to know!
Regards!
The "toolkit" you make reference to is a CodeWarrior 10.2 update, it is not an executable file, you need to install it from the CodeWarrior menu in the following manner:
1 Open CodeWarrior 10.2
2 On the upper tool menu click on help > install software
3 Click on the add button to the right of the work with address bar
4 A new window will pop up, click on the archive button and navigate to the root folder where you saved the update file and click ok