unable to install the kinetis 100Mhz tool kit for windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unable to install the kinetis 100Mhz tool kit for windows

Jump to solution
839 Views
vallinaths
Contributor II

hi

  purchased the TWR-K60D100M development and download the com.freescale.mcu10_2.Kinetis_100MHz_K10_K20_K30_K40_K50_K60.win.v1_0_2 from the freescale website and unzip the file and trying to run the content.jar executable file .and getting an error "invalid or corrupted jar file " having Jdk 6 and jre7 version java . Please let me know the solution to problem

thanks

vallinath

Labels (1)
0 Kudos
Reply
1 Solution
668 Views
apanecatl
Senior Contributor II

The "toolkit" you make reference to is a CodeWarrior 10.2 update, it is not an executable file, you need to install it from the CodeWarrior menu in the following manner:

1 Open CodeWarrior 10.2

2 On the upper tool menu click on help > install software

3 Click on the add button to the right of the work with address bar

4 A new window will pop up, click on the archive button and navigate to the root folder where you saved the update file and   click ok

View solution in original post

0 Kudos
Reply
3 Replies
668 Views
vallinaths
Contributor II

thanks works fine

0 Kudos
Reply
668 Views
Monica
Senior Contributor III

Vallinath, were this suggestions useful?

We'd like to know!

Regards!

0 Kudos
Reply
669 Views
apanecatl
Senior Contributor II

The "toolkit" you make reference to is a CodeWarrior 10.2 update, it is not an executable file, you need to install it from the CodeWarrior menu in the following manner:

1 Open CodeWarrior 10.2

2 On the upper tool menu click on help > install software

3 Click on the add button to the right of the work with address bar

4 A new window will pop up, click on the archive button and navigate to the root folder where you saved the update file and   click ok

0 Kudos
Reply