some problems on 16bit-data flexbus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

some problems on 16bit-data flexbus

ソリューションへジャンプ
2,256件の閲覧回数
guangyuanhan
Contributor I

we used 32bit address bus and 16bit data bus to connect a sram which databus is from ad0-ad15. control chip is mk60dn512zvlq10 and sram chip is cy62177. but k60 could not read the higher 8bit data of the 16bit data!    any ideas?   anyone who have proposed circiuit?  thx

0 件の賞賛
返信
1 解決策
1,970件の閲覧回数
OliverSedlacek
Contributor III

There are a lot of configuration registers that need to be set correctly to get this to work. Port muxes must be set to ALT5 or ALT6 as appropriate for the Flexbus pins FB_AD0 to FB_AD_15, FB_A0 to FB_A23, and FB control signals. You also need to configure the flexbus control pin functions so that you get a CS, WE, OE, BHE and BLE. The CSCR needs to be configured with a 16 bit port width and a suitable number of wait states.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,971件の閲覧回数
OliverSedlacek
Contributor III

There are a lot of configuration registers that need to be set correctly to get this to work. Port muxes must be set to ALT5 or ALT6 as appropriate for the Flexbus pins FB_AD0 to FB_AD_15, FB_A0 to FB_A23, and FB control signals. You also need to configure the flexbus control pin functions so that you get a CS, WE, OE, BHE and BLE. The CSCR needs to be configured with a 16 bit port width and a suitable number of wait states.

0 件の賞賛
返信
1,970件の閲覧回数
guangyuanhan
Contributor I

i have received your reply.thanks for your suggestion!

2013/6/20 OliverSedlacek <[email protected]>

**

image: Freescale Community<https://community.freescale.com/index.jspa> some

problems on 16bit-data flexbus created by OliverSedlacek<https://community.freescale.com/people/OliverSedlacek>in

Kinetis Microcontrollers - View the full discussion<https://community.freescale.com/message/335795#335795>

0 件の賞賛
返信