some problems on 16bit-data flexbus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

some problems on 16bit-data flexbus

跳至解决方案
2,309 次查看
guangyuanhan
Contributor I

we used 32bit address bus and 16bit data bus to connect a sram which databus is from ad0-ad15. control chip is mk60dn512zvlq10 and sram chip is cy62177. but k60 could not read the higher 8bit data of the 16bit data!    any ideas?   anyone who have proposed circiuit?  thx

0 项奖励
回复
1 解答
2,023 次查看
OliverSedlacek
Contributor III

There are a lot of configuration registers that need to be set correctly to get this to work. Port muxes must be set to ALT5 or ALT6 as appropriate for the Flexbus pins FB_AD0 to FB_AD_15, FB_A0 to FB_A23, and FB control signals. You also need to configure the flexbus control pin functions so that you get a CS, WE, OE, BHE and BLE. The CSCR needs to be configured with a 16 bit port width and a suitable number of wait states.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,024 次查看
OliverSedlacek
Contributor III

There are a lot of configuration registers that need to be set correctly to get this to work. Port muxes must be set to ALT5 or ALT6 as appropriate for the Flexbus pins FB_AD0 to FB_AD_15, FB_A0 to FB_A23, and FB control signals. You also need to configure the flexbus control pin functions so that you get a CS, WE, OE, BHE and BLE. The CSCR needs to be configured with a 16 bit port width and a suitable number of wait states.

0 项奖励
回复
2,023 次查看
guangyuanhan
Contributor I

i have received your reply.thanks for your suggestion!

2013/6/20 OliverSedlacek <[email protected]>

**

image: Freescale Community<https://community.freescale.com/index.jspa> some

problems on 16bit-data flexbus created by OliverSedlacek<https://community.freescale.com/people/OliverSedlacek>in

Kinetis Microcontrollers - View the full discussion<https://community.freescale.com/message/335795#335795>

0 项奖励
回复