problem to update boot loader on FRDMKL25Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

problem to update boot loader on FRDMKL25Z

跳至解决方案
2,536 次查看
lucasmahieu
Contributor III

Hello,

I really need help to update my boot loader ...

I follow all the step since 4hours ...

- i enter in bootloader mode,

- i drag and drop the BOOTUPDATEAPP_Pemicro_v111.SDA,

- i can see the led blinking

- BUT when i unplug then plug the board there are NOTHING !!!!!! my computer doesn't see nothing !

I tri with win XP on a PC, I tried with my mac, and with my win7 on virtual box on my mac.

AND I SEE NOTHING ! I think i am becoming crazy

Can you help me ? PLEAZE

标签 (1)
0 项奖励
回复
1 解答
2,394 次查看
lucasmahieu
Contributor III

Hello every body,

and a big thanks for your answers !

I found the source of the problem ... It was very stupid ...

On Win7, I draged/dropped the BOOTUPDATAPP.......SDA from the zip files. But i didn't UNZIP the directory ... so when i dragged /dropped then unplug, nothing happened ... So a unzip all the directory on the computer, and then i dragged /dropped and when i unplug then plug the device, it was seen like FRDMKL25Z mass device.

Thanks a lot

Lucas

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,395 次查看
lucasmahieu
Contributor III

Hello every body,

and a big thanks for your answers !

I found the source of the problem ... It was very stupid ...

On Win7, I draged/dropped the BOOTUPDATAPP.......SDA from the zip files. But i didn't UNZIP the directory ... so when i dragged /dropped then unplug, nothing happened ... So a unzip all the directory on the computer, and then i dragged /dropped and when i unplug then plug the device, it was seen like FRDMKL25Z mass device.

Thanks a lot

Lucas

0 项奖励
回复
2,394 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Lucas,

it is good to know it. Thanks for sharing.

Regards,

Carlos

0 项奖励
回复
2,394 次查看
Carlos_Musich
NXP Employee
NXP Employee
0 项奖励
回复
2,394 次查看
yasuhikokoumoto
Senior Contributor I

Hello,

have you installed the Windows USB Drivers "PEDrivers_install.exe"?

When you unplug then plug the board, did you not see MSD "BOOTLOADR"?

If no, it is strange.

If yes, you should also drag and drop MSD-DEBUG-FRDM-KL25Z_Pemicro_v114.SDA.

If you have already tried all, I am sorry for not helping you.

Best regards,

Yasuhiko Koumoto.

0 项奖励
回复