problem to update boot loader on FRDMKL25Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem to update boot loader on FRDMKL25Z

ソリューションへジャンプ
2,624件の閲覧回数
lucasmahieu
Contributor III

Hello,

I really need help to update my boot loader ...

I follow all the step since 4hours ...

- i enter in bootloader mode,

- i drag and drop the BOOTUPDATEAPP_Pemicro_v111.SDA,

- i can see the led blinking

- BUT when i unplug then plug the board there are NOTHING !!!!!! my computer doesn't see nothing !

I tri with win XP on a PC, I tried with my mac, and with my win7 on virtual box on my mac.

AND I SEE NOTHING ! I think i am becoming crazy

Can you help me ? PLEAZE

ラベル(1)
0 件の賞賛
返信
1 解決策
2,482件の閲覧回数
lucasmahieu
Contributor III

Hello every body,

and a big thanks for your answers !

I found the source of the problem ... It was very stupid ...

On Win7, I draged/dropped the BOOTUPDATAPP.......SDA from the zip files. But i didn't UNZIP the directory ... so when i dragged /dropped then unplug, nothing happened ... So a unzip all the directory on the computer, and then i dragged /dropped and when i unplug then plug the device, it was seen like FRDMKL25Z mass device.

Thanks a lot

Lucas

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,482件の閲覧回数
lucasmahieu
Contributor III

Hello every body,

and a big thanks for your answers !

I found the source of the problem ... It was very stupid ...

On Win7, I draged/dropped the BOOTUPDATAPP.......SDA from the zip files. But i didn't UNZIP the directory ... so when i dragged /dropped then unplug, nothing happened ... So a unzip all the directory on the computer, and then i dragged /dropped and when i unplug then plug the device, it was seen like FRDMKL25Z mass device.

Thanks a lot

Lucas

0 件の賞賛
返信
2,482件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Lucas,

it is good to know it. Thanks for sharing.

Regards,

Carlos

0 件の賞賛
返信
2,482件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee
0 件の賞賛
返信
2,482件の閲覧回数
yasuhikokoumoto
Senior Contributor I

Hello,

have you installed the Windows USB Drivers "PEDrivers_install.exe"?

When you unplug then plug the board, did you not see MSD "BOOTLOADR"?

If no, it is strange.

If yes, you should also drag and drop MSD-DEBUG-FRDM-KL25Z_Pemicro_v114.SDA.

If you have already tried all, I am sorry for not helping you.

Best regards,

Yasuhiko Koumoto.

0 件の賞賛
返信