looking for demo of adc to uart dma on Kinetis L FRDM board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

looking for demo of adc to uart dma on Kinetis L FRDM board

跳至解决方案
2,020 次查看
steve_fae
Senior Contributor I

Any working PE demos we can experiment with?

1 解答
1,404 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I believe that the best approach is to use the examples found in the installation folder of CW 10.3

C:\Freescale\CW MCU v10.3\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-KL25Z48M

I hope this helps,

Alejandro

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,405 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I believe that the best approach is to use the examples found in the installation folder of CW 10.3

C:\Freescale\CW MCU v10.3\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-KL25Z48M

I hope this helps,

Alejandro

0 项奖励
回复
1,404 次查看
steve_fae
Senior Contributor I

Basically something to compliment AN4631 but it doesn't provide a project. 

0 项奖励
回复
1,404 次查看
Monica
Senior Contributor III

Steven, is this suggestion helpful?

Please let us know! :smileywink:

0 项奖励
回复
1,404 次查看
steve_fae
Senior Contributor I

I have made a big commitment to using PE, so starting in a different path isn't where I want to go.  So still hoping for a PE example that works.  I will be passing this along to my customer after I try it myself.

1,404 次查看
deepakrana
NXP Employee
NXP Employee

hi

In these examples you have a low power UART with DMA example

http://cache.freescale.com/files/32bit/software/KL25_SC.exe?fpsp=1&WT_TYPE=BSDL&WT_VENDOR=FREESCALE...

This is not PE but will be a good starting point to use this for ADC with DMA.

0 项奖励
回复