looking for demo of adc to uart dma on Kinetis L FRDM board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

looking for demo of adc to uart dma on Kinetis L FRDM board

Jump to solution
2,052 Views
steve_fae
Senior Contributor I

Any working PE demos we can experiment with?

1 Solution
1,436 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I believe that the best approach is to use the examples found in the installation folder of CW 10.3

C:\Freescale\CW MCU v10.3\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-KL25Z48M

I hope this helps,

Alejandro

View solution in original post

0 Kudos
Reply
5 Replies
1,437 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I believe that the best approach is to use the examples found in the installation folder of CW 10.3

C:\Freescale\CW MCU v10.3\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-KL25Z48M

I hope this helps,

Alejandro

0 Kudos
Reply
1,436 Views
steve_fae
Senior Contributor I

Basically something to compliment AN4631 but it doesn't provide a project. 

0 Kudos
Reply
1,436 Views
Monica
Senior Contributor III

Steven, is this suggestion helpful?

Please let us know! :smileywink:

0 Kudos
Reply
1,436 Views
steve_fae
Senior Contributor I

I have made a big commitment to using PE, so starting in a different path isn't where I want to go.  So still hoping for a PE example that works.  I will be passing this along to my customer after I try it myself.

1,436 Views
deepakrana
NXP Employee
NXP Employee

hi

In these examples you have a low power UART with DMA example

http://cache.freescale.com/files/32bit/software/KL25_SC.exe?fpsp=1&WT_TYPE=BSDL&WT_VENDOR=FREESCALE...

This is not PE but will be a good starting point to use this for ADC with DMA.

0 Kudos
Reply