kv11 flexcan network example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

kv11 flexcan network example

1,690 次查看
jasonhaedt
Contributor III

Hello I am using the KV11 device and KSDK 1.3.  I noticed there is no flexcan network example.  There was a version started in standalone 1.2 but it did not compile.  Is Freescale working on something that they are able to share for demonstrating the flexcan interface on the KV11 device?

Thank you,

Jason Haedt

标记 (3)
0 项奖励
回复
1 回复

1,463 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,Jason,

Unfortunately, i have not the example code for FlexCan based on Kinetis, but the MC56F84xxx and Kinetis use the same FlexCAN module, I attach the example based on MC56F84xxx, so that you can refer to it.

BR

Xiangjun Rong

0 项奖励
回复