kv11 flexcan network example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kv11 flexcan network example

1,634件の閲覧回数
jasonhaedt
Contributor III

Hello I am using the KV11 device and KSDK 1.3.  I noticed there is no flexcan network example.  There was a version started in standalone 1.2 but it did not compile.  Is Freescale working on something that they are able to share for demonstrating the flexcan interface on the KV11 device?

Thank you,

Jason Haedt

タグ(3)
0 件の賞賛
返信
1 返信

1,407件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,Jason,

Unfortunately, i have not the example code for FlexCan based on Kinetis, but the MC56F84xxx and Kinetis use the same FlexCAN module, I attach the example based on MC56F84xxx, so that you can refer to it.

BR

Xiangjun Rong

0 件の賞賛
返信