k64 USB U-disk enumeration error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

k64 USB U-disk enumeration error

ソリューションへジャンプ
5,275件の閲覧回数
omercaylan
Contributor II

hi, we desing custom pcb with k64, we are trying to communite via usb, when usb disk attached, i get USB_HostEventEnumerationFail, when i examine the signal with oscilloscope, i get such a signal. Do you have any idea about this problem ? ide : McuXpresso sdk : 2.8.2WhatsApp Image 2020-11-10 at 10.51.31 AM (1).jpegWhatsApp Image 2020-11-10 at 10.51.31 AM (1).jpeg

0 件の賞賛
返信
1 解決策
5,124件の閲覧回数
omercaylan
Contributor II

Problem Solved: the schematic was wrong, . i connect 5v to k64 Usb reg. it worked.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
5,125件の閲覧回数
omercaylan
Contributor II

Problem Solved: the schematic was wrong, . i connect 5v to k64 Usb reg. it worked.

0 件の賞賛
返信
5,170件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

 

Hi

I would suggest you use USB analyzer to capture some USB packets.

Do you use OCARM or SDRAM as your first RAM in your project? Or DTCM as your first RAM?

 

Regards

Daniel

0 件の賞賛
返信
5,208件の閲覧回数
bobpaddock
Senior Contributor IV

Do the OE pins have internal pull-ups?  Such pins should not be floating.
The OSC could be randomly turning on and off.

 

0 件の賞賛
返信
5,189件の閲覧回数
omercaylan
Contributor II

actually i checked the OSCs. links like this. OSC output so I measure the clk voltage 5.1 volts, do you think this could be a mistake? OSC VDD 3.3v

omeroaylan_0-1605707673211.pngomeroaylan_0-1605707673211.png

 

0 件の賞賛
返信
5,230件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi omeroaylan:

 

Could you provide more information about your application , what changes did you make? what demo you are using?

 

Regards

Daniel

0 件の賞賛
返信
5,226件の閲覧回数
omercaylan
Contributor II

mcu : 144pin, MK64FN1M0VLQ12
we use external clock for usb and mcu. usb clk in : 47 - PTE26
we are only testing usb msd example.first we tested the code without any change on our circuit but did not work,
second we created a clean project for out 144 pin mcu and tested again(usb msd) but not a chance.
example working on nxp development board but not working our board.  i want to know, is this usb signal correct ?
it works until this function( USB_HostEvent() ) and i get enumeration error.code.pngcode.pngosi.pngosi.pngprojeicindekiler.pngprojeicindekiler.pngusb.pngusb.png

0 件の賞賛
返信