i m using twr-k40x256 but is unable to blink the led..i m constantly getting error .....2 main() main.c:14 0x1fff81e0 and ...2 main() main.c:14 0x1fff81e0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i m using twr-k40x256 but is unable to blink the led..i m constantly getting error .....2 main() main.c:14 0x1fff81e0 and ...2 main() main.c:14 0x1fff81e0

Jump to solution
1,459 Views
mithleshchaubey
Contributor I

what should i do

Labels (1)
1 Solution
1,302 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello.

I have attached an example project for CodeWarrior v10.5, on which the blue LED of TWR-K40X256 board is initialized and configured for a continuous toggle; you could use it as reference.

Hope this will be useful for you.

Best regards!

/Carlos

View solution in original post

3 Replies
1,303 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello.

I have attached an example project for CodeWarrior v10.5, on which the blue LED of TWR-K40X256 board is initialized and configured for a continuous toggle; you could use it as reference.

Hope this will be useful for you.

Best regards!

/Carlos

1,302 Views
mithleshchaubey
Contributor I

could you please tell me how to display timer from 59-0 sec on the

twrpi-slcd...

the above problem was resolved...thanks for your concern..

On Sat, Oct 5, 2013 at 5:48 AM, CarlosCasillas <

0 Kudos
Reply
1,302 Views
nasreenshaikh
Contributor III

Hi Mithlesh,

Please give more details specific to your problem. when exactly are you getting this error? At build time or run time?

paste a  sample of your code here so that we can have a look and help you with your problem.

0 Kudos
Reply