i m using twr-k40x256 but is unable to blink the led..i m constantly getting error .....2 main() main.c:14 0x1fff81e0 and ...2 main() main.c:14 0x1fff81e0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i m using twr-k40x256 but is unable to blink the led..i m constantly getting error .....2 main() main.c:14 0x1fff81e0 and ...2 main() main.c:14 0x1fff81e0

跳至解决方案
1,463 次查看
mithleshchaubey
Contributor I

what should i do

标签 (1)
1 解答
1,306 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hello.

I have attached an example project for CodeWarrior v10.5, on which the blue LED of TWR-K40X256 board is initialized and configured for a continuous toggle; you could use it as reference.

Hope this will be useful for you.

Best regards!

/Carlos

在原帖中查看解决方案

3 回复数
1,307 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hello.

I have attached an example project for CodeWarrior v10.5, on which the blue LED of TWR-K40X256 board is initialized and configured for a continuous toggle; you could use it as reference.

Hope this will be useful for you.

Best regards!

/Carlos

1,306 次查看
mithleshchaubey
Contributor I

could you please tell me how to display timer from 59-0 sec on the

twrpi-slcd...

the above problem was resolved...thanks for your concern..

On Sat, Oct 5, 2013 at 5:48 AM, CarlosCasillas <

0 项奖励
回复
1,306 次查看
nasreenshaikh
Contributor III

Hi Mithlesh,

Please give more details specific to your problem. when exactly are you getting this error? At build time or run time?

paste a  sample of your code here so that we can have a look and help you with your problem.

0 项奖励
回复