header file of TFT LCD 2.8"(CN7) for k20-50m

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

header file of TFT LCD 2.8"(CN7) for k20-50m

4,643 次查看
vahidnoori
Contributor II

hiiiii.

is there any body that can help me about header files of tft lcd 2.8" for k20-50m????:smileycry::smileycry::smileycry:

标签 (1)
标记 (2)
0 项奖励
回复
10 回复数

4,318 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Can you elaborate a bit more what you need? What TFT LCD 2.8”? What board, custom, TWR, FRDM?

Luis

4,318 次查看
vahidnoori
Contributor II
0 项奖励
回复

4,318 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

I have reviewed the Keil project in the tftlcd.zip file.

You can start with any of the examples in Sample code package (SC code) for the K20 initialization. Then, you need to rewrite/adapt the SPI.c and ADS7843.c functions code for K20 peripherals (SPI).

Best Regards,

Luis

0 项奖励
回复

4,318 次查看
vahidnoori
Contributor II
0 项奖励
回复

4,320 次查看
vahidnoori
Contributor II

Hi dear.

Can u solve my problem

Sent from my HTC

0 项奖励
回复

4,320 次查看
vahidnoori
Contributor II

Dear luis.

Can u adapt this files for k20? The other file should be adapted. It is dificult

Sent from my HTC

0 项奖励
回复

4,319 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

What is the connection between FRD-K20 and the LCD board? Is it a LCD Arduino Shield?

Best Regards,

0 项奖励
回复

4,319 次查看
vahidnoori
Contributor II

On Wed, Oct 30, 2013 at 2:10 PM, Luis Casado

0 项奖励
回复

4,319 次查看
vahidnoori
Contributor II
0 项奖励
回复

4,319 次查看
vahidnoori
Contributor II

my board is FRDM-K20D50M .and i am  going to config graphic LCD by this microcontroller .but i have not the header file of this LCD for FRDM .  can u help me? my TFT lcd is CN7

0 项奖励
回复