header file of TFT LCD 2.8"(CN7) for k20-50m

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

header file of TFT LCD 2.8"(CN7) for k20-50m

4,575 Views
vahidnoori
Contributor II

hiiiii.

is there any body that can help me about header files of tft lcd 2.8" for k20-50m????:smileycry::smileycry::smileycry:

Labels (1)
Tags (2)
0 Kudos
Reply
10 Replies

4,250 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Can you elaborate a bit more what you need? What TFT LCD 2.8”? What board, custom, TWR, FRDM?

Luis

4,250 Views
vahidnoori
Contributor II
0 Kudos
Reply

4,250 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

I have reviewed the Keil project in the tftlcd.zip file.

You can start with any of the examples in Sample code package (SC code) for the K20 initialization. Then, you need to rewrite/adapt the SPI.c and ADS7843.c functions code for K20 peripherals (SPI).

Best Regards,

Luis

0 Kudos
Reply

4,250 Views
vahidnoori
Contributor II
0 Kudos
Reply

4,252 Views
vahidnoori
Contributor II

Hi dear.

Can u solve my problem

Sent from my HTC

0 Kudos
Reply

4,252 Views
vahidnoori
Contributor II

Dear luis.

Can u adapt this files for k20? The other file should be adapted. It is dificult

Sent from my HTC

0 Kudos
Reply

4,251 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

What is the connection between FRD-K20 and the LCD board? Is it a LCD Arduino Shield?

Best Regards,

0 Kudos
Reply

4,251 Views
vahidnoori
Contributor II

On Wed, Oct 30, 2013 at 2:10 PM, Luis Casado

0 Kudos
Reply

4,251 Views
vahidnoori
Contributor II
0 Kudos
Reply

4,251 Views
vahidnoori
Contributor II

my board is FRDM-K20D50M .and i am  going to config graphic LCD by this microcontroller .but i have not the header file of this LCD for FRDM .  can u help me? my TFT lcd is CN7

0 Kudos
Reply