hardware multiply speed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hardware multiply speed

ソリューションへジャンプ
1,712件の閲覧回数
Florijan
Contributor III

Hi,

can any one tells me is the speed of hardware multiply 1 cycle or 32 cycle version in Kinetis L type of MCUs?  I was reading on the internet that there are two hardware choices for multiply. The first is 1 cycle an the other is 32 cycle version for lower cost designs. Which of this versions is supported in Kinetis L MCUs?

Best regards,

Florijan

ラベル(1)
0 件の賞賛
返信
1 解決策
1,475件の閲覧回数
sNilesh
Contributor III

Hello,

Kinetic - L supports : Single cycle 32 bits by 32 bits multiply

You can follow : KL04/KL05 Product Brief, Rev. 2, 6/2012

Page no : 12.

Link : http://cache.freescale.com/files/32bit/doc/prod_brief/KL05PB.pdf?fpsp=1

----------------------------------------------------------

For more information on : Cortex-M multiply you can go through : ARM Cortex-M - Wikipedia, the free encyclopedia

Thanks,

Nilesh

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,476件の閲覧回数
sNilesh
Contributor III

Hello,

Kinetic - L supports : Single cycle 32 bits by 32 bits multiply

You can follow : KL04/KL05 Product Brief, Rev. 2, 6/2012

Page no : 12.

Link : http://cache.freescale.com/files/32bit/doc/prod_brief/KL05PB.pdf?fpsp=1

----------------------------------------------------------

For more information on : Cortex-M multiply you can go through : ARM Cortex-M - Wikipedia, the free encyclopedia

Thanks,

Nilesh

0 件の賞賛
返信