hardware multiply speed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

hardware multiply speed

跳至解决方案
1,241 次查看
Florijan
Contributor III

Hi,

can any one tells me is the speed of hardware multiply 1 cycle or 32 cycle version in Kinetis L type of MCUs?  I was reading on the internet that there are two hardware choices for multiply. The first is 1 cycle an the other is 32 cycle version for lower cost designs. Which of this versions is supported in Kinetis L MCUs?

Best regards,

Florijan

标签 (1)
0 项奖励
回复
1 解答
1,004 次查看
sNilesh
Contributor III

Hello,

Kinetic - L supports : Single cycle 32 bits by 32 bits multiply

You can follow : KL04/KL05 Product Brief, Rev. 2, 6/2012

Page no : 12.

Link : http://cache.freescale.com/files/32bit/doc/prod_brief/KL05PB.pdf?fpsp=1

----------------------------------------------------------

For more information on : Cortex-M multiply you can go through : ARM Cortex-M - Wikipedia, the free encyclopedia

Thanks,

Nilesh

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,005 次查看
sNilesh
Contributor III

Hello,

Kinetic - L supports : Single cycle 32 bits by 32 bits multiply

You can follow : KL04/KL05 Product Brief, Rev. 2, 6/2012

Page no : 12.

Link : http://cache.freescale.com/files/32bit/doc/prod_brief/KL05PB.pdf?fpsp=1

----------------------------------------------------------

For more information on : Cortex-M multiply you can go through : ARM Cortex-M - Wikipedia, the free encyclopedia

Thanks,

Nilesh

0 项奖励
回复