Kinetis K10 datasheet discrepancy - MCG_C1 --> IREFS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K10 datasheet discrepancy - MCG_C1 --> IREFS

1,425件の閲覧回数
ignisuti
Contributor IV

I'm curious if there is a discrepancy on page 528 of the Manual. 


It says that IREFS value for MCG_C1 selects either the External Reference Clock or the slow internal reference clock.

But, if MCG_C2 --> IRCS is configured to use the Fast internal reference clock, then IREFS would be fast, not slow... right?

0 件の賞賛
返信
2 返答(返信)

1,182件の閲覧回数
apanecatl
Senior Contributor II

To use the Fast internal reference clock you only need to set IRCS as Fast Internal Reference Clock enabled (1), the state of IREFS is irrelevant once you set IRCS

0 件の賞賛
返信

1,182件の閲覧回数
kidfy
Contributor I

yes, but before you select the fast clock mode, you need check the FRDIV ,and make sure the clock source for FLL is between 31.25khz-39.025khz.

0 件の賞賛
返信