eGUI using K70's LCDC and any TFT LCD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eGUI using K70's LCDC and any TFT LCD

2,059 次查看
ángelbarragán
Contributor I

Hi,

     I'm fairly new to the programming of Freescale's microcontrollers and for a project that I will soon start working on, the intention is to implement the K70's LCDC with any TFT LCD. I see that there is a software library called eGUI, however, all the eGUI implementation examples that I've seen on the web only include the K70 twr-kit and the twr-lcd or twr-lcd-RGB module. My question is: Is it possible to implement eGUI with any K70's LCDC and any TFT LCD without using twr kits? Thanks in advance.

标签 (1)
2 回复数

1,839 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Of course, you can. You can reuse everything except the particular parameters of your TFT panel and resize the frame buffer to the panel resolution. See attached file.

Luis

1,839 次查看
ángelbarragán
Contributor I

Hello Luis,

     First of all I would like to thank you for your fast response. It really help me out a lot. One last question, if the K70 already has an LCDC, then I must purchase an TFT LCD without a controller like the SSD1963, right? Thanks for taking your time in responding my questions.

Ángel

0 项奖励
回复