eGUI release

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

eGUI release

跳至解决方案
41,404 次查看
Thommi_Tulpe
Contributor IV

Hi Gargy,

when can I use the new release of the eGUI.

You told the bug in the console is fixed.

If the release is not ready, can I change the files d4d_console.c and d4d_console.h  in the old version of the eGUI

with your help ?

 

Best Regards

Thomas

1 解答
38,966 次查看
Gargy
NXP Employee
NXP Employee

I'm so sorry to tell that but we don't have plan to add this to version 3.00. You can try to do it your self, in final this will be compounded object from edit box, button and list box (list box contains scroll bar).

Temporary you can use MENU or List box and for simply replace just comment the old object definition and create new one with same name.

The eGUI I will send to you on email.

Gargy

在原帖中查看解决方案

55 回复数
7,146 次查看
lh_dan
Contributor III

Hi

I would also love to evaluate eGUI 3.00 for an upcoming project.  Could I please get a copy?

-Dan

0 项奖励
回复
7,146 次查看
Gargy
NXP Employee
NXP Employee

Please send me in private message your email, it will be nice just for info some info about your project.

GArgy

7,145 次查看
Tuna
Contributor I

Hi Petr,

İf it is possible please send me a last release of eGui.

[email protected]

Thank you.

0 项奖励
回复
7,146 次查看
lh_dan
Contributor III

Petr,

Seems like we need to be 'friends' in order to send you a private message?  Is this right?  I would be glad to send you info about my project.

-Dan

0 项奖励
回复
7,142 次查看
Gargy
NXP Employee
NXP Employee

Hi,

maybe :-), I really don't know. But good point - I found about 8 requests from others to be friends .

7,140 次查看
lh_dan
Contributor III

Hi Petr,

Could you send me eGUI v3.0?

[email protected]

Thanks,

Dan

0 项奖励
回复
7,141 次查看
antonio66
Contributor III

Hi Peter,

I'm developing a project with TWR_K60N512 and the egui 2.1

I would like to evaluate eGUI 3.00 for my project.  Could I please get a copy?

Antonio


0 项奖励
回复
7,142 次查看
Gargy
NXP Employee
NXP Employee

Hi,

yes I can, send me a your email.

Gargy

7,141 次查看
leepenn
Contributor III

Hi Petr,

     If possible I would also like a copy of egui v3.0 for evaluation.

     [email protected]

Thank You,

Lee

0 项奖励
回复
7,141 次查看
antonio66
Contributor III

Hi Peter,

this is my personal email address.

You can also send here the

link to nuew egui.

Thank you very much

best regards

Antonio Brignoli

-


Messaggio originale----

Da: [email protected]

Data:

06/02/2013 9.00

A: "antonio brignoli"<[email protected]>

Ogg: Re:

Kinetis Microcontrollers - eGUI release

Petr Gargulak [https:

//community.freescale.com/people/Gargy] created the discussion

"eGUI

release"

To view the discussion, visit: https://community.freescale.

com/message/314731#314731

0 项奖励
回复
7,142 次查看
lh_dan
Contributor III

Hi Petr,

Were you able to get the private message I sent to you?

-Dan

0 项奖励
回复
7,142 次查看
michris
Contributor III

Dear Petr,

Is it possible to also send me the latest version of eGui please. ([email protected])

My application is a console for controlling electrical charging stations.

Many thanks in advance

Regards,

Michris

0 项奖励
回复
7,142 次查看
Toe
Contributor IV

I would like to use the updated version as well.  Can you send a copy to [email protected]?

Thanks

0 项奖励
回复
7,142 次查看
roelblomjous
Contributor I

Hi, I want to use eGUI 3.00 to create a gui for a wvga display using the TWR-K70F120M.
my email address is [email protected]

Regards,

Roel


0 项奖励
回复