eGUI Unicode build errors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

eGUI Unicode build errors

跳至解决方案
9,753 次查看
seandema
Contributor IV

I'm attempting to use unicode with eGUI(D4D). Everything works fine when just using ASCII but I can't get things to compile once I #define D4D_UNICODE. I've never used unicode before so there is probably just something I'm missing. I'm running on a Kinetis K70 with MQX 4.1 with the eGUI 3.01 from github Gargy007/eGUI · GitHub​ all building in CodeWarrior 10.6. Here is a sample of my code.

#include "wchar.h"

const wchar_t * ws = L"Wide string";

D4D_WCHAR english[] = {L"English"};

Line 3 has the error: unknown type name 'wchar_t'

Line 3 has the error: wide character array initialized from incompatible wide string

From what I understand I need the 'L' before my string to make it a long string but that doesn't seem to help.

Does anyone know what I've done wrong.

Thanks,

Sean

标签 (1)
0 项奖励
回复
1 解答
9,021 次查看
EarlOrlando
Senior Contributor II

Hello Sean,

I was working with IAR, whose compiler interprets the short and int type variables different. I compiled a demo in CW and I got the same error, the solution was change the D4D_WCHAR type variable.

In the file "d4d_types.h" you have to change the D4D_WCHAR typedef from unsigned short to unsigned int.

From:

#ifndef D4D_WCHAR

  typedef unsigned short D4D_WCHAR; 

#endif 

To:

#ifndef D4D_WCHAR

  typedef unsigned int D4D_WCHAR; 

#endif 

I hope this solve your problem.

Regards,

Earl Orlando.

/* If this post solve your problem please click the Correct Answer button. */

在原帖中查看解决方案

0 项奖励
回复
14 回复数
9,021 次查看
EarlOrlando
Senior Contributor II

Hello Sean,

Please include the file "d4d.h"

#include "d4d.h"

Where is included the file "d4d_types.h", where is defined the data type "D4D_TCHAR", please use it.

#include "d4d.h"

const D4D_TCHAR * ws = L"Wide string"

D4D_TCHAR english[] = {L"English"};

Regards,

Earl.

0 项奖励
回复
9,021 次查看
seandema
Contributor IV

Thanks for the suggestion but it is still not working. Here is my code.

#include "d4d.h"

#include "fonts.h"

#include "main.h"

const D4D_TCHAR * ws = L"Wide string";   

D4D_TCHAR english[] = {L"English"};

Line 05 is now a warning instead of an error. The warning is "initialization from incompatible pointer type [enabled by default]".

Line 06 is still an error. The error is "wide character array initialized from incompatible wide string".

That got me a little closer to a fix but still not working.

Please let me know if you have any more suggestions.

Thanks,

Sean

0 项奖励
回复
9,021 次查看
EarlOrlando
Senior Contributor II

Are you sure you have the next definition?

#define D4D_UNICODE

Try with the following code, please:

#include "d4d.h" 

#include "fonts.h" 

#include "main.h" 

D4D_TCHAR ws[] = {D4D_DEFSTR("Wide string")};

D4D_TCHAR english[] = {D4D_DEFSTR("English")};

Regards,

Earl.

0 项奖励
回复
9,021 次查看
seandema
Contributor IV

Yes, I have #define D4D_UNICODE in my d4d_user_cfg.h file.

Gave the above code a try but that't not working for me either. Both lines now have the error "wide character array initialized from incompatible wide string".

Is it possible I have something setup wrong with CodeWarrior or my project properties? I'm just not sure what that would be since commenting out #define D4D_UNICODE removes all these build errors.

Thanks,

Sean

0 项奖励
回复
9,021 次查看
EarlOrlando
Senior Contributor II

Are these lines in your file "d4d_types.h"?

#ifndef D4D_WCHAR_TYPE

/*! @brief User type definition of eGUI wide char.*/

  #define  D4D_WCHAR_TYPE unsigned short

#endif

/*! @brief Type definition of eGUI wide char.*/

typedef D4D_WCHAR_TYPE D4D_WCHAR;

/*! @brief Type definition of eGUI ASCII character.*/

typedef char D4D_CHAR;

#ifdef D4D_UNICODE

  /*! @brief Type definition of eGUI character (it depends on UNICODE setting if this is \ref D4D_CHAR or \ref D4D_WCHAR).*/

  typedef D4D_WCHAR D4D_TCHAR;

#else

  /*! @brief Type definition of eGUI character (it depends on UNICODE setting if this is \ref D4D_CHAR or \ref D4D_WCHAR).*/

  typedef D4D_CHAR D4D_TCHAR;

#endif

Regards,

Earl.

0 项奖励
回复
9,021 次查看
seandema
Contributor IV

Yes those lines are in my d4d_types.h file. I even copied into beyond compare to be sure. Mine code is on the left and your code is on the right.

pastedImage_3.png

Thanks,

Sean

0 项奖励
回复
9,022 次查看
EarlOrlando
Senior Contributor II

Hello Sean,

I was working with IAR, whose compiler interprets the short and int type variables different. I compiled a demo in CW and I got the same error, the solution was change the D4D_WCHAR type variable.

In the file "d4d_types.h" you have to change the D4D_WCHAR typedef from unsigned short to unsigned int.

From:

#ifndef D4D_WCHAR

  typedef unsigned short D4D_WCHAR; 

#endif 

To:

#ifndef D4D_WCHAR

  typedef unsigned int D4D_WCHAR; 

#endif 

I hope this solve your problem.

Regards,

Earl Orlando.

/* If this post solve your problem please click the Correct Answer button. */

0 项奖励
回复
9,021 次查看
vittorio-castel
Contributor II

Hello Earl Orlando,

I am using the D4D eGui Library with KDS 3.0 for a K20 project.

I found the same solution as yours, changing the D4D_TCHAR from unsigned short to unsigned int, as GDB assumes the wide-chars as 4-bytes characters (such as in Linux environment; Windows, instead, considers the L"...." strings as 2-bytes per character strings).

Have you any suggestion for converting UTF8 strings (received from a communication) to the correct UNICODE format for eGui? Actually I just copy the 1-byte per char UTF8 string to a 4-bytes per character D4D_TCHAR, but when it finds a 2-bytes character in the UTF-8 string, it is not correctly displayed (lowercase accented 'a' becomes a uppercase 'A' with tilde). Only 1-byte characters are correctly displayed.

I used the Freescale Embedded Gui Converter utility to create the font choosing Unicode-16bit encoding and including the Latin and 2 Latin-extended Unicode ranges.

Thanks in advance for any suggestion.

Vittorio

0 项奖励
回复
9,021 次查看
vittorio-castel
Contributor II

Hello again, I found a solution for converting strings from UTF8 to 4-bytes per character UNICODE strings, so now I can display correctly all the 2-bytes UTF8 symbols.

Sorry for bothering.

Best wishes,

Vittorio

9,021 次查看
EarlOrlando
Senior Contributor II

Hello Vittorio,

Could you please share your solution?

Best regards,

Earl.

0 项奖励
回复
9,021 次查看
vittorio-castel
Contributor II

Hello Earl,

this is the function I used for converting strings from uint8_t * UTF8 format to uint32_t UNICODE (TCHAR when D4D_UNICODE is enabled in eGui):

void utf8ToTCHAR(unsigned int *dst, uint8_t *src) {

  while (*src) {

    if (*src < 0x80) { // 0x0-7F range

      *dst++ = *src++;

    } else if (*src > 0b10111111) { // 0x80-7FF range

       *dst = (*src & 0x1F) << 8; // first byte

       *dst = (*dst | ((*(src+1) & 0b00111111) << 2)) >> 2; // second byte

       src += 2;

       dst++;

     }

   }

   *dst = 0; // string terminator

}

Cheers,

Vittorio

9,021 次查看
seandema
Contributor IV

That fixed it!

Thanks so much for all your help. I really appreciate it.

Sean

0 项奖励
回复
9,021 次查看
EarlOrlando
Senior Contributor II

Hello Sean,

I am currently working to solve that.

Regards,

Earl.

0 项奖励
回复
9,021 次查看
seandema
Contributor IV

Hello Earl,

Thanks for looking into this. If you find a fix please let me know.

Luckily it's not a feature I need immediately for my current project. Just wanted to be sure I'll be able to use it later when I do need it.

Thanks,

Sean

0 项奖励
回复