regarding MII and RMII interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

regarding MII and RMII interface

1,464件の閲覧回数
shivakumarlv
Contributor I

HI everyone

I am using freescale K70 series microcontroller (part number MK70FN1M0VMJ12) I have interfaced Ethernet switch IC ( part number LAN9303i) in MII. Whether Can I use this physical interface in RMII mode by keeping MII pins remain connected or I need to make NC( not connected ). Please confirm on this

Awaiting your reply

Regards,

Shiva kumar L V

Hardware Design Engineer - EE Excellence center,

Dover -IIC,

Web site:www.dovercorporation.com

Bangalore

Ph :-8050138478,

Skype ID :- [email protected]

0 件の賞賛
返信
1 返信

1,332件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

There is no problem to keep MII pin connected (customer can set MII related pin with another function or keep the default setting at Pin Control Register n (PORTx_PCRn) register [MUX] bits).

The RMII operates at 50 MHz and requires synchronization between the PHY and the ENET RMII interface clock input(EXTAL).

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信