currently Iam using MKM34Z128ACLL5 is any bootloader application for this controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

currently Iam using MKM34Z128ACLL5 is any bootloader application for this controller

3,078 Views
bharthyalla
Contributor I

I have Sample code of Serial boot loader.i done some modifications and after compiling and executing. sending the .SREC(Motorola) format file through serial interface communication tool and its Restarting to the Main function.     

2 Replies

2,708 Views
MarMi
NXP Employee
NXP Employee

Hello,

you can also refer to attached bootloader workshop document for more information on how to use AN2295 with Kinetis-M. Download training examples from here: TWR-KM34Z75M training examples. Application named "_boot_example" shows all modifications in linker file that needs to be made to allow flashing application using AN2295 bootloader.

Kind regards,

Martin M. 

0 Kudos
Reply

2,708 Views
miduo
NXP Employee
NXP Employee

Hi,

What the sample code you mean? Does the AN2295SW:

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN2295SW.zip

Has you ever download the M bare-metal drivers and software examples

https://www.nxp.com/webapp/sps/download/preDownload.jsp