currently Iam using MKM34Z128ACLL5 is any bootloader application for this controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

currently Iam using MKM34Z128ACLL5 is any bootloader application for this controller

2,056件の閲覧回数
bharthyalla
Contributor I

I have Sample code of Serial boot loader.i done some modifications and after compiling and executing. sending the .SREC(Motorola) format file through serial interface communication tool and its Restarting to the Main function.     

2 返答(返信)

1,687件の閲覧回数
MarMi
NXP Employee
NXP Employee

Hello,

you can also refer to attached bootloader workshop document for more information on how to use AN2295 with Kinetis-M. Download training examples from here: TWR-KM34Z75M training examples. Application named "_boot_example" shows all modifications in linker file that needs to be made to allow flashing application using AN2295 bootloader.

Kind regards,

Martin M. 

0 件の賞賛
返信

1,687件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

What the sample code you mean? Does the AN2295SW:

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN2295SW.zip

Has you ever download the M bare-metal drivers and software examples

https://www.nxp.com/webapp/sps/download/preDownload.jsp