common mode range

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

common mode range

2,033 次查看
jakebailey
Contributor I

What is the common mode input range of K22 differential ADC? I assumed it would be reasonably close to the supply rails but this does not appear to be the case as inputting common mode signals above 1.2 vref starts to cause distortion.

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,943 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

You can find the VADIN in DataSheet.

VADIN.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,943 次查看
jakebailey
Contributor I

This is still a bit ambiguous as there is also a pin on the package labeled VREFH which I have tied to 3v3 but I am using internal 1.2v reference so is max VADIN 31/32 of 1.2v (selected VREF) or 31/32 of 3.3V (package pin).

0 项奖励
回复

1,943 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

ADC Reference Options.png

ADCx_SC2[REFSEL] bit selects the voltage reference sources for ADC.
When 1.2 V VREF_OUT is selected, the The max VADIN is 31/32 of 1.2v.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复