common mode range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

common mode range

2,139件の閲覧回数
jakebailey
Contributor I

What is the common mode input range of K22 differential ADC? I assumed it would be reasonably close to the supply rails but this does not appear to be the case as inputting common mode signals above 1.2 vref starts to cause distortion.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,049件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

You can find the VADIN in DataSheet.

VADIN.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,049件の閲覧回数
jakebailey
Contributor I

This is still a bit ambiguous as there is also a pin on the package labeled VREFH which I have tied to 3v3 but I am using internal 1.2v reference so is max VADIN 31/32 of 1.2v (selected VREF) or 31/32 of 3.3V (package pin).

0 件の賞賛
返信

2,049件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

ADC Reference Options.png

ADCx_SC2[REFSEL] bit selects the voltage reference sources for ADC.
When 1.2 V VREF_OUT is selected, the The max VADIN is 31/32 of 1.2v.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信