clk out to drive ic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,923件の閲覧回数
bilgekaanugur
Contributor II

I need a clock source ( 8-16 mhz ) to  feed ic .  what is the suitable method in ke04 family to generate this ?  

ラベル(2)
1 解決策
1,836件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

1. Using PTH2 output bus clock. You can also enable bus clock output via an optional prescaler.

bus clock output.png

2. Using "Output Compare mode" of FTM module. It can be configured to Toggle mode.

Output Compare mode.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,837件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

1. Using PTH2 output bus clock. You can also enable bus clock output via an optional prescaler.

bus clock output.png

2. Using "Output Compare mode" of FTM module. It can be configured to Toggle mode.

Output Compare mode.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

1,836件の閲覧回数
bilgekaanugur
Contributor II

thank you Robin for your prompt reply.

regards

0 件の賞賛
返信