clk out to drive ic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

clk out to drive ic

Jump to solution
1,114 Views
bilgekaanugur
Contributor II

I need a clock source ( 8-16 mhz ) to  feed ic .  what is the suitable method in ke04 family to generate this ?  

1 Solution
1,027 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

1. Using PTH2 output bus clock. You can also enable bus clock output via an optional prescaler.

bus clock output.png

2. Using "Output Compare mode" of FTM module. It can be configured to Toggle mode.

Output Compare mode.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,028 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

1. Using PTH2 output bus clock. You can also enable bus clock output via an optional prescaler.

bus clock output.png

2. Using "Output Compare mode" of FTM module. It can be configured to Toggle mode.

Output Compare mode.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

1,027 Views
bilgekaanugur
Contributor II

thank you Robin for your prompt reply.

regards

0 Kudos
Reply