can_loopback_demo wont work on twrk60d100m

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can_loopback_demo wont work on twrk60d100m

1,162 次查看
yarannan
Contributor III

Hi,

I used CWU 10.6 to run can demo project with twr-k60d100m with twr-ind-io. The issue is it wont send message. It only sits there try to read.

Does anybody know what happened there?

0 项奖励
回复
3 回复数

1,045 次查看
mnorman
NXP Employee
NXP Employee

Hi, Yaran,

Which software are you trying to run?  MQX demo?

-Michael

0 项奖励
回复

1,045 次查看
yarannan
Contributor III

can_loopback_demo on K60 tower

0 项奖励
回复

1,045 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Yaran,

Do you mean the demo which under the CW10.6 ( "...\CW MCU v10.6\MCU\CodeWarrior_Examples\Kinetis_Examples\k60\can_loopback_node")?

If yes , please refer the "can_loopback_node.txt"(...\CW MCU v10.6\MCU\CodeWarrior_Examples\Kinetis_Examples\doc) .

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

0 项奖励
回复