can_loopback_demo wont work on twrk60d100m

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can_loopback_demo wont work on twrk60d100m

1,190件の閲覧回数
yarannan
Contributor III

Hi,

I used CWU 10.6 to run can demo project with twr-k60d100m with twr-ind-io. The issue is it wont send message. It only sits there try to read.

Does anybody know what happened there?

0 件の賞賛
返信
3 返答(返信)

1,073件の閲覧回数
mnorman
NXP Employee
NXP Employee

Hi, Yaran,

Which software are you trying to run?  MQX demo?

-Michael

0 件の賞賛
返信

1,073件の閲覧回数
yarannan
Contributor III

can_loopback_demo on K60 tower

0 件の賞賛
返信

1,073件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Yaran,

Do you mean the demo which under the CW10.6 ( "...\CW MCU v10.6\MCU\CodeWarrior_Examples\Kinetis_Examples\k60\can_loopback_node")?

If yes , please refer the "can_loopback_node.txt"(...\CW MCU v10.6\MCU\CodeWarrior_Examples\Kinetis_Examples\doc) .

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

0 件の賞賛
返信