bulid ucosii failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,295件の閲覧回数
dugg
Contributor II

hello everyone:

i have downloaded the file:

Micrium_FRDM-K64F_OS2-KSDK.zip.when i build it with KDS,  it show: 

error: unrecognized command line option '-nanolibc'


0 件の賞賛
返信
1 解決策
2,205件の閲覧回数
BlackNight
NXP Employee
NXP Employee

It seems that this project was for an old version of KDS (probably v1.0?) with an old GNU toolchain. The most recent version is V3.2.0 and it uses the option --specs=nano.specs instead:

pastedImage_1.png

See as well Switching ARM GNU Tool Chain and Libraries in Kinetis Design Studio | MCU on Eclipse 

I hope this helps,

Erich

元の投稿で解決策を見る

2 返答(返信)
2,206件の閲覧回数
BlackNight
NXP Employee
NXP Employee

It seems that this project was for an old version of KDS (probably v1.0?) with an old GNU toolchain. The most recent version is V3.2.0 and it uses the option --specs=nano.specs instead:

pastedImage_1.png

See as well Switching ARM GNU Tool Chain and Libraries in Kinetis Design Studio | MCU on Eclipse 

I hope this helps,

Erich

2,205件の閲覧回数
dugg
Contributor II

thanks for your answer!!!

0 件の賞賛
返信